This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SATA link down (SStatus 0 SControl 310)

Guru 20755 points

Other Parts Discussed in Thread: OMAP3530

Hello,

I receive the following failure when connecting sdd:

.....

CPSW phy found : id is : 0x282f014

PHY 0:04 not found
IP-Config: Guessing netmask 255.0.0.0
IP-Config: Complete:
device=eth0, addr=10.0.0.2, mask=255.0.0.0, gw=255.255.255.255,
host=10.0.0.2, domain=, nis-domain=(none),
bootserver=255.255.255.255, rootserver=10.0.0.1, rootpath=
PHY: 0:01 - Link is Up - 100/Full
ata1: COMRESET failed (errno=-32)
ata1: limiting SATA link speed to 1.5 Gbps

Link not established, limiting speed

ata1: SATA link down (SStatus 0 SControl 310)
EXT3-fs: barriers not enabled

Do you have any idea what it means ?

Thanks, Ran