I need to read the MAC address (during Kernel init) from serial EEPROM which is an I2C device. I appreciate any pointers to existing code or similar implementation.
My environment: AM335x, ATMEL EEPROM (AT24C01B) 2-wire I2C serial device.
Thanks
Hay
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need to read the MAC address (during Kernel init) from serial EEPROM which is an I2C device. I appreciate any pointers to existing code or similar implementation.
My environment: AM335x, ATMEL EEPROM (AT24C01B) 2-wire I2C serial device.
Thanks
Hay
Hi Hay,
Here is an example from the SDK 06.00.00.00. This is from the am335x_evm_setup() function inside the board-am335xevm.c file:
/* 1st get the MAC address from EEPROM */
ret = mem_acc->read(mem_acc, (char *)&am335x_mac_addr,
EEPROM_MAC_ADDRESS_OFFSET, sizeof(am335x_mac_addr));
if (ret != sizeof(am335x_mac_addr)) {
pr_warning("AM335X: EVM Config read fail: %d\n", ret);
return;
}
/* Fillup global mac id */
am33xx_cpsw_macidfillup(&am335x_mac_addr[0][0],
&am335x_mac_addr[1][0]);
Best regards,
Miroslav