Hi All,
In AM437x GP EVM, only one row keypad buttons are working. Remaining two row buttons are not working.
Row GPIO pins
We are getting IRQ for GPIO bank 3. For these reason GPIO_3_21 key pad buttons are working. We are not getting IRQ for GPIO_4_3 and GPIO_4_2. I mean to say IRQ is not received for GPIO Bank 4. For these reason remaining 4 buttons are not working.
SW4 -- working
SW5 -- Not working
SW6 - Not working
SW7 - working
SW8 - Not working
SW9 - not working.
I found this issue with both Linux SDK( kernel version 3.12) and row-boat android 4.3. In both cases only SW4 and SW7 button is working. Remaining 4 buttons are not working.
Also I cross checked with Diagnostic software. there all the key pad buttons are working.
Does anybody face same issue on AM437X GP EVM?
Regards,
Yuvaraj