Other Parts Discussed in Thread: OMAP-L138, AES-128, OMAPL138
I have a customer asking -
Does enabling encryption affect the max speed at which we can run the part?
I haven't found any documentation that addresses this question.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ignacio,
What type of encryption are you talking about ?
ie Secure part or something else (At linux side ?) ?
What is the processor are customer using ?
AES-128. Military application, so customer wants to validate/encrypt software image. OMAP-L138.
Hi Ignacio,
I presume that you are not using secure OMAPL138 processor.
Does enabling encryption affect the max speed at which we can run the part?
In my understanding, No.
http://software-dl.ti.com/tsu_encryption/tsu_encryption_public_sw/index.html
If you are not using the secure OMAPL138 part then I would like to suggest to use secure OMAPL138 processor (only C6748 DSP core secured) which is using AES-128 encryption.
http://processors.wiki.ti.com/index.php/Basic_Secure_Boot_for_OMAP-L138_C6748