This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CONNECT TLV320AIC29 TO OMAPL137



Hi

I have a new system with omapl137. i used tlv320aic29 in my board. tlv320aic29 connected to omapl137 with spi1 and mcasp1. i attached the shematic.

i connected the headphone to (INT_MIC+ and MIC_GROUND) and the speaker to (AF-OUT+ and AF-OUT-).

i used mcasp1 of omapl137 for loopback on tlv320aic29.

i send below command for configuration respectively, with spi1 of omapl137:

PAGE 1 CONTROL REGISTER MAP
address           command
0x04                 0xbb00
0x00                 0x1f70
0x01                 0x4000
0x02                 0x0000
0x03                 0x0001
0x0a                 0x0fff
0x0b                 0x0000
0x0c                 0x0404
0x0d                 0x0012

PAGE2 CONTROL REGISTER MAP
address           command
0x00                 0x413f
0x01                 0x8000
0x02                 0x0080
0x03                 0x8030
0x04                 0x0802
0x05                 0x29c3
0x06                 0x0800
0x1b                 0x8118
0x1c                 0x0000
0x1d                 0x3fc0
0x1e                 0x3a76
0x1f                  0x8040
0x20                 0xa003
0x21                 0x00c8
0x22                 0x0004
0x23                 0x0000
0x24                 0x2800
0x25                 0x5d20
0x26                 0xffe0
0x27                 0x0000

when i power on  the board, I heard the horn from the speaker but when i reset the board i can heard the my voice from the speaker correctly. i think that something wrong in shematic or configuration.

Please help me to fix this problem.

 

 

TLV320AIC29-OMAP.pdf
  • Hi,

    Thanks for your post.

    I think, the cause of this issue could be because of your reset circuit in the schematics which is attached in your previous post. We are following it up on your previous post for the same issue and let me close this post. In order to better address your issue, please don't create any duplicate  posts for the same issue in moving forward and we are closing this post. 

    You could follow it up on the same issue in the below post:

    http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/p/363580/1277299.aspx#1277299

    Thanks & regards,

    Sivaraj K

    -------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question

    -------------------------------------------------------------------------------------------------------

  • Hi

    I fixed the reset circuit based on proposed block diagram but my problem is still not resolved.

    Please help me to fix this problem. 

    Thank you

     

  • Hello Mahdi,

    Since this thread is closed, i request you to create a new thread and post the same query again for better followup.

    Thanks for your understanding.

    Regards,
    Senthil