I'm using OMAP5 EVM and Toshiba's TC358743. I'd like to add a resolution to the EDID structure (EDID 1.3).
The resolution (1024x768) is mentioned in Established Timing section. If I set the corresponding bit in the EDID, I'm not able to get the camera handle itself. This behaviour is same for setting anything in Established Timings and Standard Timings section. What does this behaviour imply? Generally, is it possible to modify Established Timings and Standard Timings sections?
My second question is whatever resolution I mention in EDID, will all of it be supported by the Toshiba bridge?