This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error while running DVSDK 2.10 Demos for DM365

Hi all

I have succesfully completed all steps of

GSG: DM365 DVEVM Software Setup for MontaVista Kernel,

and while running the demos from the target command prompt,

i am getting following errors while executing the loadmodules_hd.sh

---------------------------------------------------------------------------------------

cmemk: disagrees about version of symbol struct_module
irqk: disagrees about version of symbol struct_module
insmod: error inserting 'cmemk.ko': -1 Invalid module format
insmod: error inserting 'irqk.ko': -1 Invalid module format
edmak: disagrees about version of symbol struct_module
insmod: error inserting 'edmak.ko': -1 Invalid module format
dm365mmap: disagrees about version of symbol struct_module
insmod: error inserting 'dm365mmap.ko': -1 Invalid module format

 

the packages used are,



dvsdk_dm365_setuplinux_2_10_01_18.bin
mvl_5_0_0_demo_lsp_setuplinux_02_10_00_08.bin
xdctools_setuplinux_3_10_03.bin
mvl_5_0_demo_sys_setuplinux.bin
psp_02_10_00_08.bin

I am not sure why it is giving me such an errors and i am not able to execute the demos( encoder ,decoder , encoder+decoder )

can anyone tell me why such errors are coming and  how to solve it ..to run the demos.

Thanks.