This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can I use so-dimm SDRAM with No ECC ??

Hello

I have a XTCIEVMk2X EVM Board.  and I wan to  use new so-dimm SDRAM with no ECC.

I had to exchange so-dimm SDRAM from basically provided SDRAM to ordinary SDRAM using lap top

but I can't see kernel message because U-BOOT is no running.

U-BOOT have new error message, "DDR Leveling Error Detected!"

Can I use this SDRAM??

Regards.