This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

a high pcie load will affect dm8168's whole performance?

Hi,TIer.

I have a general problem,not a specific one.

If I use DM8168 with a heavy pcie load,such as use FPGA to transfer HD video frame to dm8168,or dm8168 send HD video frame to C6678,or a Gbit Ethernet pcie card connected,or something else.A heavy pcie load will affect dm8168's whole performance?such as the m3 video's h.264 encode/decode,or M3 vpss's scaler?

I think pcie's inbound/outbound memory is mapped to DDR.And for DDR's control,M3 video/vpss has the most priority for ddr controller.And if pcie module uses ddr for a large time interval,will affect m3's performance?

My understanding is right or wrong?

THANKS!BR!