Hey,
Bios 6.4 TiRTOS 2.02.36 CCS6
1. Main:
// ....Set FPU
FPULazyStackingEnable();
FPUEnable();
/* *** *** START BIOSU *** *** */
//System_printf("exit main()\n");
//Breakpoint One
BIOS_start(); /* does not return */
return(0);
}
2. FPCC = 0xC0000000
3. The problem is that after BIOS start, FPCC=0x0000000 .And FPU does not work properly - sometimes are calculating errors.
4. When i add lines AFTER BIOS started:
FPUEnable();
FPULazyStackingEnable();
FPU works properly and calculations are good.
So question: Is is normal that BIOS clear fpu config? Can i call FPULazyStackingEnable() after bios started?