This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Grace 3.0 Timer interval miscalculated when using timer divisor



When using Interval mode and a timer clock source divisor, it seems that Grace 3.0 miscalculates the interval. 

ACLK=8192 Hz, Desired Interval=200 mS, Clock Divisor=4. 

Generated Code:

TIMER_A_configureUpMode(TIMER_A1_BASE, TIMER_A_CLOCKSOURCE_ACLK, TIMER_A_CLOCKSOURCE_DIVIDER_4,
1637, TIMER_A_TAIE_INTERRUPT_DISABLE, TIMER_A_CCIE_CCR0_INTERRUPT_ENABLE, TIMER_A_SKIP_CLEAR);

-----------------------------------------------

Timer1_A3.timerMode = xdc.module("ti.mcu.msp430.csl2.timer.ITimer").IntervalMode;
Timer1_A3.intervalModeActive = true;
Timer1_A3.compareValue[0] = 101;
Timer1_A3.regs.interruptSource[1].interruptEnable = true;
Timer1_A3.regs.interruptSource[1].interruptHandler = true;
Timer1_A3.intervalModeAdvanced = true;
Timer1_A3.TACTL.timerClockSourceDivider = xdc.module("ti.mcu.msp430.csl2.timer.ITimer_A").TIMERA_CLOCKSOURCE_DIVIDER_4;
Timer1_A3.regs.interruptSource[0].interruptHandler = true;
Timer1_A3.regs.interruptSource[2].interruptHandler = true;
Timer1_A3.regs.interruptSource[3].interruptHandler = true;

Timer1_A3.inputClockToTimer = 8.192;

Timer1_A3.intervalDesiredPeriod = 200.0;
Timer1_A3.pwmDesiredFrequency = 5.0;

  • Bug 3024 Timer interval miscalculated when using timer divisor has been submitted. This will be resolved in Grace 3.00.01.

    I believe you can work around this by setting the Divider before setting the Desired Interval  Period.

    Regards,

    Joe