Other Parts Discussed in Thread: TPS53313
Hi Team,
I'm using the TMDSDC3359 to do some development. But it suddenly lost the control from serial console yesterday. I'm so sorry that I didn't save the logging message before close the TeraTerm window.
I've checked the cable and the COM port of PC, they are all normal. The only difference from my previous using is the original 12V power adapter is replaced with a 15V-1.25A one. But even with this one, the board has been worked normally for about 4 hours. When the problem appeared, I was doing the data transfer testing.
Now, after power on, the LED on the PLC SOM does not blink and none LED on the whole board blink. No any message come from the serial console.
Can you please suggest what's wrong with the board and how to resolve the problem?
Thanks a lot!
Best Regards,
Jeanne Yi