This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Library error on Ramdisk image (DVEVM)



HI, everyone.

We have tried to test ramdisk image for encode demo program. The following error message is launched when staring encode demo program.

-----------------------------------------------------------------------------------------------------------------

CMEMK module: built on Sep 18 2009 at 00:39:17
Starting portmap  Reference Linux version 2.6.18
 daemon: portmap  File /home/user/dvsdk_2_00_00_22/linuxutils_2_23_01/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c
/etc/rc.d/rcS.d/S41portmap: 156: nice: not found
pidof: invalid option -- x
BusyBox v1.01 (2005.12.18-04:57+00ioremap_nocache(0x87600000, 10485760)=0xc8000000
00) multi-call ballocated heap buffer 0xc8000000 of size 0x2c000
inary

No helpcmem initialized 5 pools between 0x87600000 and 0x88000000
 available.

.
dsplinkk: no version for "struct_module" found: kernel tainted.
DSPLINK Module (1.61.03) created on Date: Apr 16 2009 Time: 18:22:23
INIT: Entering runlevel: 3
Starting internet superserver: inetd.

MontaVista(R) Linux(R) Professional Edition 4.0.1 (0502020)

(none) login: root


Welcome to MontaVista(R) Linux(R) Professional Edition 4.0.1 (0502020).

login[416]: root login  on `console'

# cd /opt/dm6446/
# ./ODU -v test.mpeg4 -o
./ODU: relocation error: /lib/libpthread.so.0: symbol errno, version GLIBC_PRIVATE not defined in file libc.so.6 with link time reference
#

-----------------------------------------------------------------------------------------------------------------

We copied some libraries from my workspace for ODU(encode demo proram). But we cannot run ODU.

How can we solve this problem? Would you give me some informat about it?

Thank you and BR.

Lee.