Other Parts Discussed in Thread: DM388
Hi,
I am developing applications on DM388 based on Appro's RDK.
However, I found that once the application exited, a reboot was needed to run it again.
Otherwise there would be errors from VPSS.
I looked into the system_server and ipnc_rdk_mcfw.out source code in order to dig out the proper init and deinit procedure.
I put all the init and deinit commands to script files.
The attached initall.sh is what I use to initialize the system and unload.sh is used to do deinit.
So after the system boots up, I run initall.sh (under /opt/ipnc) and everything seems to go well.
Then I can run my application.
After the application exits, I try running unload.sh and that is when the problem occurs.
I have logged the terminal output into the attached error.log file.
Could you help look into the issue?
What I see from the log seems to indicate that the problem is due to inproper deinit in VPSS.
All the files are attached. 3731.files.zip
Thank you.