Other Parts Discussed in Thread: TMS320DM6437
Hello,
I'm an electronic engineer, I have to make a prototype of printed circuit based in EVM TMS320DM6437, its dimension is (38mm*38mm*5mm), this circuit will be integrated in a camera ( VCA (Video Content Analytics) module is intelligent video solution for video surveillance), the problem is that I must take some bloc diagram from the 34 sheets of the DM6437 technical reference, the board must have: the core DM6437, Nand and Nor falsh interfaces, DDR2 memory interface, the power bloc and the reset supervisor bloc, as I said before this board will be integrated in a camera: it will have an SPI communication with an ARM9 (ARM is master and the EVM is slave) also the board will be interfaced with a CCD sensor.
My question is : The datasheet of EVM contain 34 bloc sheets, extracting only these blocs can ensure me the best fonction of the module, if no which are the module should I add to ensure this fonction
Thanks