Hi experts,
I did some tests about PCIe on ti-linux-3.12.y, the top commit is the following
commit 5c62fd05f12d008a136d5620d12a76d50429af3c
Merge: cd57586 d83a323
Author: Dan Murphy <DMurphy@ti.com>
Date: Fri Aug 1 12:28:06 2014 -0500
[ 25.095717] pinctrl-single 4a003400.pinmux: 281 pins at pa fc003400 size 1124
[ 25.097146] ### dra7xx_pcie_probe 318
[ 25.097839] ### dra7xx_pcie_link_up 103 reg 0 x0 Link_up 0x10000
[ 25.097847] ### dra7xx_pcie_establish_link 118
[ 25.310381] dra7xx-pcie 51002000.pcie: link is not up
[ 25.310608] PCI host bridge to bus 0000:00
It seems PCIe link is not up, if there is anything wrong with my operations?
I secured a E1000e PCIe network card in the board.
Cheers,
Zumeng