This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDMI input support

Hi there,

Does anyboday know that besides DM8168, are there any other type of Davinci video processors having HDMI input interface?

Thx~~~

BR,

-Yongying

  • Hi,

    Non Davinci device has built-in HDMI interface. What we have is video port which is 8/16/24 bit width w/ embedded/discrete sync.

    I am not sure what your question really is.  Are you just looking for any Davinci based ref design which can demo HDMI input?

    BR,

    Eason

  • Hi Eason,

    We are looking for the Davinci based design to support video input of HDMI and SD/HD-SDI. We already have the design on DM8168 for HDMI interface using Sil9135. Actually there are two questions:

    First, we are looking for the reference design on DM8168 to support SD/HD-SDI video input.

    Second, I was wondering if there are any alternatives to DM8168 that can do above jobs?

    Many thx~~~

    -Yongying

       

  • Hi

     For SDI HD deisgn, pls refer to http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/337424.aspx

    For alternatives of DM8168,  TI provides DM8148. DM8127/DM385 etc.

    Please go to DM8148 product side for the details.

    BR,

    Eason