Other Parts Discussed in Thread: OMAP-L138, ADS8558
I use the OMAP-L138 and an ADS8558.
They are linked through the uPP.
On GPIO bank 6 I generate the CONVST, CS, RD (ADS) and ENABLE, CLOCK (uPP) signals.
The uPP-STARTA Signal is disabled (UPICR).
CS, RD and CLOCK are driven by one GPIO together.
The dma-descriptor is configured to get 6 words:
if (!CSL_FEXT(upp0Regs->UPIS2, UPP_UPIS2_PEND)
&& !CSL_FEXT(upp0Regs->UPIS2, UPP_UPIS2_ACT))
upp0Regs->UPID0 = (uint32_t) &uppInputBuffer;
upp0Regs->UPID1 = CSL_FMK(UPP_UPID1_LNCNT, 1)
| CSL_FMK(UPP_UPID1_BCNTH, 6);
upp0Regs->UPID2 = (0);
}
But the following loop exits after 11 cycles:
// CLK/RD until EOLI/EOWI/ERROR:
while (upp0Regs->UPIER == 0) {
// CLK/CS/RD low:
*gpio_bank6_out_data = gpio_b6_state[state_ADS_CONVST_H_ADS_CS_L_UPP_EN_L];
// CLK/CS/RD high:
*gpio_bank6_out_data = gpio_b6_state[state_ADS_CONVST_H_ADS_CS_H_UPP_EN_L];
}
In uppInputBuffer[0]..[5] are the datas, uppInputBuffer[6] is untouched, but the datas are at wrong order:
I have to reorder it whith this statement:
inputData[0] = uppInputBuffer[4]);
inputData[1] = uppInputBuffer[5]);
inputData[2] = uppInputBuffer[0]);
inputData[3] = uppInputBuffer[1]);
inputData[4] = uppInputBuffer[2]);
inputData[5] = uppInputBuffer[3]);
My questions:
1.) Why it takes 11 clocks?
2.) Why it is in wrong order?
Can help somebody?
Andreas
--
PS. uPP conf:
// uPP Channel Control Register
upp0Regs->UPCTL = CSL_FMKT(UPP_UPCTL_MODE, RECEIVE)
| CSL_FMKT(UPP_UPCTL_CHN, ONE)
| CSL_FMKT(UPP_UPCTL_SDRTXIL, DISABLE)
| CSL_FMKT(UPP_UPCTL_DDRDEMUX, DISABLE)
| CSL_FMKT(UPP_UPCTL_DRA, SINGLE) | CSL_FMKT(UPP_UPCTL_IWA, 16BIT)
| CSL_FMKT(UPP_UPCTL_DPWA,FULL);
// uPP Interface Configuration Register
upp0Regs->UPICR = CSL_FMKT(UPP_UPICR_STARTA, DISABLE)
| CSL_FMKT(UPP_UPICR_ENAPOLA, INVERT) | CSL_FMKT(UPP_UPICR_ENAA, ENABLE)
| CSL_FMKT(UPP_UPICR_CLKINVA, NORMAL)
| CSL_FMKT(UPP_UPICR_STARTPOLA, INVERT);
// idle value register
upp0Regs->UPIVR = CSL_FMKT(UPP_UPIVR_VALA, RESETVAL);
// uPP Threshold Configuration Register
upp0Regs->UPTCR = CSL_FMKT(UPP_UPTCR_RDSIZEI, 64B);
// uPP Interrupt Enable Set Register
upp0Regs->UPIES = CSL_FMKT(UPP_UPIES_EOLI, SET)
| CSL_FMKT(UPP_UPIES_EOWI, SET);
// DLB:
CSL_FINST(upp0Regs->UPDLB, UPP_UPDLB_BA, DISABLE);
CSL_FINST(upp0Regs->UPDLB, UPP_UPDLB_AB, DISABLE);
// uPP Peripheral Control Register
CSL_FINST(upp0Regs->UPPCR, UPP_UPPCR_EN, ENABLE);