Hello,
I've attached a HDMI receiver to the DM8168, using the 24bit VIP0A, Hsync, Vsync and the clock.
My input is 1080p60 or 720p60, my input signals seem ok and are described here: http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/p/362772/1286420.aspx
My horizontal line including blanking is longer than 11 bits (it's 2200px), so the VIP reports 0x98 (wraps). Will this cause issues?
Which OMX API call can I use to put the VIP in clipping mode, i.e. count only the active video pixels/lines? Will this reflect in the VIP size register?
How can I set the polarity of Hsync/Vsync in OMX?
Regards,
Lo