This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Default GTF Support in EDID



I'm using EDID 1.3 in the TC358743 Toshiba HDMI2CSI bridge for OMAP5.

I'd like to add a new resolution which is not provided by VESA and CEA. If I need to add it in the Standard Timing descriptor section, do I have to enable or disable anything in the Feature support section (or anywhere else in the EDID)? For example, there is Default GTF support and Secondary GTF support. If I enable Default GTF Support, will that mean that all the timings (including VESA and CEA supported) will be calculated based on GTF method only? Or only the PC resolutions I have mentioned in the standard timing section will be calculated based on GTF?