Other Parts Discussed in Thread: TMS320C6748
In a space-constrained design, is it allowable (from the point of view of TI silicon) to tie inputs which are required to be static high (e.g. dedicated Boot pins, unused NMI, etc) directly to the appropriate supply rail (i.e. without using a pull-up resistor)?
I realise that the use of resistors has advantages i.t.o. being able to mod the board if required, but assuming that the design is settled, pin allocation is fixed and software can be 'guaranteed' not to accidentally set these pins to "output low", is it allowable to tie inputs hard high (just as it is to tie static low input pins directly to GND)?
The industry in general seems to differentiate between TTL inputs (where the use of pull-ups in these situations is generally advised) and CMOS inputs (where inputs tied hard high seem to be allowable). It would be great to have an authoritative generic reply for all TI parts on this, but in case this needs to be more specific, the part in question today is a TMS320C6748 DSP which has (dual-voltage capable) LVCMOS inputs.