This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to install user build linux kernel modules on SD-Card



Hi All,

I am working on TI-Linux SDK for AM335x Starter kit.

have done some changes in usb/gadget.zero.c file.

i have created .ko and .o files for that.

 When i tried to load this modules on SD card with "Modules_install command", i can see that the modules that are installed in rootfs/lib/modules/kernel/drivers/usb/gadget folder are the one which come with standard SDK pack.

when i run modinfo on the prepared SDcard (by entering in /media/rootfs/......) for g_zero.ko file i see the details as those are built for ARMv6,

but if i see the modinfo on the SDK of ti (home/igate/ti-sdk-directory/usb/gadget/) for the same file g_zero.ko isee the details a those are build for ARMv7.

What should be the steps to follow to install the modified modules on SD card?

Thanks in advance.....