This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

(Very Urgent) Unable to connect CCSv5.5 using GDBserver

Hello Sir,

We have configured the CCS using telnet and tried to connect with the EVM (AM5777), but the GDB debug launcher hangs at 57%. We verified that telnet works fine when tested through command prompt and also we ensured that the GDB server agent  is running on the EVM. Please find the snapshots below depicting the configuration done and error encountered.

We need this connectivity to debug the linux application running on ARM cores.

As per the procedure the GDB connectivity with the server can be obtained through SSH or Telnet. Since SSH is not responding for the requests we tried using Telnet.

Please provide your feedback/ suggestions to resolve the same. 

We have posted the problem faced using SSH in another forum :

http://e2e.ti.com/support/omap/f/885/p/365870/1287163.aspx#1287163

Thanks,

Naveen Shetti

  • Naveen,

    The CCS configuration itself looks ok to me, although I am not an expert specifically on the AM5777 EVM and how the connection with the server is to be set up through SSH or Telnet. I think the experts in the OMAP forum would be in a better position to advice on this, so I will move this thread to the OMAP forum.