/**********************************************************/
/* */
/* LINKER command file for LEAD3 memory map */
/* */
/**********************************************************/
MEMORY
{
PAGE 0:
MMR : origin = 0000000h, length = 00000c0h
SPRAM : origin = 00000c0h, length = 0000040
DARAM0 : origin = 0000100h, length = 0003F00h
DARAM1 : origin = 0004000h, length = 0004000h
DARAM2 : origin = 0008000h, length = 0004000h
DARAM3 : origin = 000c000h, length = 0004000h
SARAM0 : origin = 0010000h, length = 0004000h
SARAM1 : origin = 0014000h, length = 0004000h
SARAM2 : origin = 0018000h, length = 0004000h
SARAM3 : origin = 001c000h, length = 0004000h
SARAM4 : origin = 0020000h, length = 0004000h
SARAM5 : origin = 0024000h, length = 0004000h
SARAM6 : origin = 0028000h, length = 0004000h
SARAM7 : origin = 002c000h, length = 0004000h
SARAM8 : origin = 0030000h, length = 0004000h
SARAM9 : origin = 0034000h, length = 0004000h
SARAM10 : origin = 0038000h, length = 0004000h
SARAM11 : origin = 003c000h, length = 0004000h
SARAM12 : origin = 0040000h, length = 0004000h
SARAM13 : origin = 0044000h, length = 0004000h
SARAM14 : origin = 0048000h, length = 0004000h
SARAM15 : origin = 004c000h, length = 0004000h
CE0 : origin = 0050000h, length = 03b0000h
CE1 : origin = 0400000h, length = 0400000h
CE2 : origin = 0800000h, length = 0400000h
CE3 : origin = 0c00000h, length = 03f8000h
PDROM : origin = 0ff8000h, length = 07f00h
VECS : origin = 0ffff00h, length = 00100h /* reset vector */
}
SECTIONS
{
vectors : {} > VECS PAGE 0 /* interrupt vector table */
.cinit : {} > SARAM0 PAGE 0
.text >> PDROM
isrs : {} > SARAM2 PAGE 0
.stack : {} > DARAM0 PAGE 0
.sysstack: {} > DARAM0 PAGE 0
.sysmem : {} > DARAM1 PAGE 0
.data : {} > DARAM1 PAGE 0
.bss : {} > DARAM1 PAGE 0
.const : {} > DARAM1 PAGE 0
.coeffs : {} > DARAM2 PAGE 0
.dbuffer : {} > DARAM3 PAGE 0
files : {} > DARAM2 PAGE 0 /* User-defined sections */
statvar : {} > DARAM2 PAGE 0
statarry : {} > DARAM2 PAGE 0
tempvar : {} > DARAM2 PAGE 0
temparry : {} > DARAM2 PAGE 0
}
Everyone
I am working with TMS320c5515 ezdsp usbstick board.I want to load my code on onchip rom such that upon reset my application code should run instead of USB_stick_sample code which is preloaded with the board.I tried to edit the .text section of linker file with PDROM but my ccs4 is showing error.I dnt know really how can i run my application code upon reset.i dnt want to use any external memory for my application code as it is quite small in size.Please anyone help me with this.
I have attached my linker file below.
With regards
Arun