This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB0 OTG/HOST



Hi ,

Iam using OMAPL137 ,usb0 as a Host/OTG device , from the datasheet i understand that USB0_VBUS is an input to sence 5V ,But is it cumpolsary to provide 5V to USB0_VBUS  for the Controller to work as HOST mode, when a self powered device is connected to the Host .