Hello
When I run "WMAFileSeek (msec)", and is called the "WMAFileCBGetData(offset, num_bytes) ", it is run the function repeatedly, it does not end.
By the parameter to be set to "WMAFileSeek() ", this behavior occurs.
Are there any restrictions, such as the value of this parameter?
Is there a cause to the other?
Is there a known bug in the decoder of WMA?
Version:
WMA Decoder on C55x Version 01.00.00