This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about AM437x Interrupt

Guru 15520 points

Hi,

I have questions about AM437x Interrupt.

1.
In AM437x datasheet(sprs851) page.3, there are following information:
////////////////////////////////////////////////////////////////////////////////
Up to Three External DMA Event Inputs That Can Also be Used as Interrupt Inputs
////////////////////////////////////////////////////////////////////////////////

But in page.83  "4.3.12 Miscellaneous", it seem that there are
9 External DMA Event or Interrupt Inputs.
Which is true?

2.
Does AM437x support FIQ interrupt?
I'm asking this question because it was unsupported in AM335x.

3.
Is only two interrupt lines(FIQ and IRQ) connected to Cortex-A9?

4.
AM437x supports 224 shared peripheral interrupts(SPI).
I guess that user need to assign SPI to FIQ or IRQ.
There are no information in AM437x Technical Reference Manual.
Is there any information?

best regards,
g.f.