I am running DSP/BIOS 5.42.1.09 on a F28M35H52C1, com) with CCS compiler V6.1.0.A11101 (as recommended for PLC G3 development) on CCS5.5.0.00077. Occasionally, and I have seen this on as many as 10 or 40 boards, when I am requesting information from a node, the C28 appears to hang. pausing the debugger (XDS560V2 STM USB) at FXN_N_selfLoop().
First of all, where is there a manual that explains this function?
Secondly, any idea why this would occur? Why would a task end up in selfLoop?
It doesn't appear to be a stack issue, ROV shows my 5 tasks not overrunning their stack allocation. I have attached screen shots
Any input would be appreciated.
Thanks,
Pat