This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Max GPMC Clock Freq.



Is it safe to assume that the the maximum GPMC clock frequency for the OMAP5x EVM is determined by the DPLL_CORE frequency (1500MHz) divided by 8 (or 187MHz)?

This information came from the "Data Manual Operating Condition Addendum v0.6" document.

  • Hi Michael,

    The following information is presented regarding GPMC_FCLK in the Data Manual Operating Condition Addendum v0.6 (http://www.ti.com/lit/ug/swpu329/swpu329.pdf): 

    Max value of GPMC_CLK is 265.92MHz, when CORE OPP is OPP_NOM.

    Best Regards,

    Yordan