This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

connected tlv320aic29 to omapl137 with spi1 and mcasp1

Other Parts Discussed in Thread: TLV320AIC29

Hi 

I have a new system with omapl137. I used tlv320aic29 in my board. this codec connected to omapl137 with spi1 and mcasp1. I attached the shematic.

I connected headphone to (INT_MIC+ and MIC_GROUND) and speaker to (AF-OUT+ and AF-OUT-).

I used mcasp1 for loopback.

I send below command with spi1 for configuration respectively.

PAGE 1 CONTROL REGISTER MAP 
address           command
0x04                 0xbb00
0x00                 0x1f70
0x01                 0x4000
0x02                 0x0000
0x03                 0x0001
0x0a                 0x0fff
0x0b                 0x0000
0x0c                 0x0404
0x0d                 0x0012

PAGE2 CONTROL REGISTER MAP 
address           command
0x00                 0x413f
0x01                 0x8000
0x02                 0x0080
0x03                 0x8030
0x04                 0x0802
0x05                 0x29c3
0x06                 0x0800
0x1b                 0x8118
0x1c                 0x0000
0x1d                 0x3fc0
0x1e                 0x3a76
0x1f                  0x8040
0x20                 0xa003
0x21                 0x00c8
0x22                 0x0004
0x23                 0x0000
0x24                 0x2800
0x25                 0x5d20
0x26                 0xffe0
0x27                 0x0000

when i power on  the board, I heard the horn from the speaker but when i reset the board i can heard my voice from the speaker correctly. I fixed the reset circuit based on below proposed block diagram.

http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/363580.aspx

when i power on my board everything is ok, but this problem is still not resolved. I think that something wrong in shematic or configuration.

Please help me to fix this problem.

Regards,

Mahdi

TLV320AIC29-OMAP.pdf