Hi,
I am working on DM8127 RDK3.5, with Low power, 512MB Memory to complete my usecase of 4 channel (H.264 Encoded data) streaming.
My usecase is like - Capture / Encode 4 channel (H.264) / Streaming of 4 H.264 Channels.
1080p + D1 + 1080p + D1
I got a final Encoded output of 2 1080p channels and 2 D1 channels like,
[m3video] CH | In Recv In Skip In User Out Latency
[m3video] Num | FPS FPS Skip FPS FPS Min / Max
[m3video] --------------------------------------------
[m3video] 0 | 30 0 0 30 89 / 124
[m3video] 1 | 15 0 0 15 93 / 128
[m3video] 2 | 30 5 0 24 109 / 142
[m3video] 3 | 15 0 0 15 111 / 140
But, I am not able to do streaming of 4 channels...
Where are the changes required ??
Can DM8127 IPNC RDK Version 3.5 - supports 4 channel streaming?
Please help on it.
Regards,
Sandip Gokani.