This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[C6711] Audio Output Channel Select Help

Good day, I need help with an software application in Code Composer Studio using a 6711 dsp with no daugther card, only the ad535 included audio codec, to send the audio collected throught the mono line in using a microphone, to either left or right channel of the speakers connected in the line out through the 3.5mm jack. Any help will be greatly appreciated, thanks...

  • After we get your answer, I may move this thread to the "TMS320C6000™ Floating-point DSPs" forum under "Digital Signal Processors".

    This is a pretty old board, so recent example files may be hard to come by. I no longer have CCS 2.2 installed on my computer, but from some old file history it looks like there could be a DSP/BIOS-based audio example under c:\ti\examples\dsk6711\bios\audio if you are using CCS 2.2 with the DSK6711.

    If not, please supply a little more information about your board and CCS version and DSP/BIOS version you are using.