This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Recovery DM8148 with ubuntu

Hi,


I'm working on dm8148 and I would like to resinstall the ubuntu. Thus, I connected the serail port to the board in order to recover it from minicom/teraterm, running the teraterm script to recover the board.

However, It doesn't work. In particular, when I send the uboot via xmodem just after turning on the board, the transfer stucks at 1.8%: it doesn't complete.

In case I run the tftpboot commands to load the kernel and the targetfs from nfs, the ubuntu starts but it stops loading during the boot.

Any idea?

Regards,

Alessandro