This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interrupt not coming when mcspi uses FIFO in DMA mode



Hi,

I am working on mcspi whith FIFO and DMA enabled for a Beaglebone board. I am using spidev_test application(Documentation/spi/spidev_test.c) for data transfer and for reception using loopback(MISO to MOSI).

Problems:-
1: When using MCSPI_TX0 and MCSPI_RX0 registers transfer stops at wait_for_completion and no tx and rx call back is happening.


2: With reference to TRM for module control while using DMA with FIFO enabled one register FDDA is used. This register is used when a FIFO is managed by the module and DMA connected to the controller provides only 256-bit aligned address. If this bit is set the enabled channel which uses the FIFO has its data managed through MCSPI_DAFTX and MCSPI_DAFRX registers instead of MCSPI_TX(i) and MCSPI_RX(i) registers.


 From this reference when i have used MCSPI_DAFTX and MCSPI_DAFRX (Address for MCSPI_DAFTX = 0x80 and MCSPI_DAFRX = 0xa0) insted of MCSPI_TX0 and MCSPI_RX0 and set FDAA to one at module control setup.


 In this case dma_tx_callback is coming but before tx_callback getting error message "DMA synchronization event drop occurred with device 35". After tx_callback DMA transfer and reception started (because using loopback) but EOW timed out(endof word count) for transmition and because of EOW rx_callback is not happing. Below reference code for interrupt

                if (tx != NULL) {
            wait_for_completion(&mcspi_dma->dma_tx_completion);
                dma_unmap_single(&spi->dev, xfer->tx_dma, count, DMA_TO_DEVICE);
               
            if (mcspi->fifo_depth != 0) {
                        irqstat_reg = mcspi->base + OMAP2_MCSPI_IRQSTATUS;
                        if (mcspi_wait_for_reg_bit(irqstat_reg,
                                OMAP2_MCSPI_IRQ_EOW) < 0)
                                dev_err(&spi->dev, "EOW timed out\n");
                        mcspi_write_reg(mcspi->master, OMAP2_MCSPI_IRQSTATUS,
                                    OMAP2_MCSPI_IRQ_EOW);
                    }
        }

So i want to know how to enable interrupt.