On 5409. Output looks great. Can drive a PC directly from it but my TTL to convertor(s) inverts the signal. How do I reverse the polarity of the output (BDX). Same for BDR.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
On 5409. Output looks great. Can drive a PC directly from it but my TTL to convertor(s) inverts the signal. How do I reverse the polarity of the output (BDX). Same for BDR.
Hi,
Team is working on and will address your request shortly.
Thanks & regards,
Sivaraj K
Thanks.
I might have to do so, but I hope not.
McBSP has so many features that surely I am just missing it.
The reason I have this issue is that the TTL/RS-232 converters I have found invert the signal. Whereas the PC can accept my DSP's 3.3V characters direct connect on a short cable, I am too concerned about overvoltage to connect directly to receive.
Are you aware of such a converter that does not invert the signal?