Other Parts Discussed in Thread: TMS320C6748, OMAP-L138
Hi everyone, I'm pretty new to the dsp board and want to write filter related algorithms for audio signal processing.
However I've tried 3 days and still encounter problems while building project. Here's how I do this:
I'm using the TMS320C6748 DSP development Kit(LCDK) with the XDS100v2 USB emulator, CCS v5.I downloaded
omap L138_support file and OMAP-L138_GEL_BSL_Files from wiley and logPD(from omap eXperiment download
resources). And my workspace contains these
two folders.
1. In the CCS target configuration,I choose:
L138_eXperimenter_v2.ccxml
2. add files to the project I built:
L138_LCDK_aic3106_init.c
L138_LCDK_aic3106_init.h
vectors_intr.asm
linker_dsp.cmd
3. In the project properties, I set:
Include option ..\bsl\inc and ..\L138_support
file search path, add library ..\bsl\lib\evmomapl138_bsl.lib
4. turn on the power, connect the XDS100v2, switch the dip #2,3,4 on and the others off and reset the board
my code here
however, while building the allpass filter code, there are some errors
Can anyone help me on this? Thank yyyou!