This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Boot Configuration Pins

Hi,

In our custom board, the boot config pins (GPIO-14 and GPIO-15) is not reflected in DEV_Stat register after device power on. Even if boot config pins (GPIO-14 and GPIO-15) are driven high, DEV_Stat register respective bits shows "0" .

Remaining boot config pins (GPIO-1 and GPIO-13) values are reflected properly in DEV_Stat register.

Any constraints on boot config pins at POR.

Regards,

Senthil Kumar.G