This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI communication

Other Parts Discussed in Thread: TMS320DM6437

In fact, I'm working in a project aiming to realise a board based in TMS320DM6437 this board will be integrated in a camera so I need to realise a communication between the DSP DM6437 and an ARM9 (SPI communication) the DM6437 is the slave and the ARM9 is the master. First step I tryed to test the communiction between the DM6437 and an SPI EEPROM but I haven't an SPI EEPROM . So, I want to know if there is a software released by Texas instrument which helps me to make a simulation of the data transmitted from the DM6437  (with the SPI communication to ARM9) or from the DM6437 to the SPI EEPROM...

Also I want to know what would be the code configuration when I use the SPI communication between the DM6437 (slave) and ARM9 (master)
scincerely,