Hi,
In the AM335x StarterWare V2.00.01.01 ethernet example code in the file "cpswif.c" there is the following code at the end of the transmit interrupt handler:
send_head = txch->send_head;
curr_bd = send_head;
}
CPSWCPDMAEndOfIntVectorWrite(cpswinst->cpdma_base, CPSW_EOI_TX_PULSE);
cpswif_rxbd_alloc(cpswinst);
}
The question is, is the last function call "cpswif_rxbd_alloc(...)" really necessary? As this only allocates new free receive buffer decriptors I think it is not necessary to call in the transmit interrupt as there is no change in receive buffer descriptor chain.
Any ideas from TI side?
Thanks and best regards,
Patrick