This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

streaming audio from audio encoder



I'm attempting to stream audio over rtp from the audio encoder.  I've proven that the audio encoder works by sending the data from the encoder to a file and then playing that file - it works fine.

I'm using the ortp library provided (0.14.2).

I'm sending the audio encoder data using the following code:

static int encoder_audio_cb( void *bufp, int len )
{

  int n;

   n = rtp_session_send_with_ts( encoder_audio_rtp, bufp, len,
                      encoder_audio_ts );
    encoder_audio_ts += 1024/*len*/;

}

encoder_audio_cb is called from the audio encoder code when the audio encoder has a buffer to be emptied.

I'm using the following sdp

v=0
o=- 653 1 IN IN4 10.0.3.247
s=CPN-5600 streaming audio
t=0 0
m=audio 10004 RTP/AVP 96
c=IN IP4 10.0.1.202                                                           
a=rtpmap:96 mpeg4-generic/48000/2
a=fmtp:96 streamtype=5;profile-level-id=15;mode=AAC-hbr;config=1190;sizeLength=13;indexLength=3;indexDeltaLength=3;constantDuration=1024
a=control:trackID=2

I can see data being transmitted to port 10004 by using tcpdump, but the decoder (vlc) doesn't seem to see anything.  I can successfully send video using a similar setup, but audio does not work at all.

Any suggestions?