This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Main Power Failure on K2HEVM

Hi all,

The LCD displayed  "Main Power Failure" on K2HEVM. My rescue steps as follows.

1. Update BMC to latest version 1.0.2.5

    Here was my console log.

=~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2014.09.18 17:38:28 =~=~=~=~=~=~=~=~=~=~=~=

BMC>    
             

BMC VERSION 1.0.2.5
BUILT May 14 2013 11:46:18
---------------------

BMC>    [00:00:00]  BMC>    BMC Init BMC>    Begin
BMC>    [00:00:00]  BMC>    BMC Version BMC>    1.0.2.5BMC>    
BMC>    [00:00:00]  BMC>    XTCIEVMK2X
BMC>    [00:00:00]  BMC>    3.1
BMC>    [00:00:00]  BMC>    S/N: 94621
BMC>    [00:00:00]  BMC>    BMC Init BMC>    Complete
BMC>    [00:00:00]  BMC>    Main PWR Start BMC>    Begin
BMC>    [00:00:00]  BMC>    EVM setup has encountered the following error: The signal MAIN_POWER_GOOD has failed to assert
BMC>    [00:00:00]  BMC>    Main PWR Stop BMC>    Begin
BMC>    [00:00:00]  BMC>    Main PWR Stop BMC>    Complete
BMC>    [00:00:01]  BMC>    HWDBG is set to ON, evm setup will now halt.
BMC>    [00:00:01]  BMC>    To alter this behavior, please use the hwdbg command.
BMC>ver       
[00:00:03]  BMC>ver
BMC>    [00:00:03]  BMC>    Executing command "ver"
BMC>    [00:00:03]  BMC>    
BMC>    [00:00:03]  BMC>    BMC Version    EVM Type    EVM Superset    EVM Subset    EVM Version    EVM S/N        UCD Ver
BMC>    [00:00:03]  BMC>    1.0.2.5        0.0.0.1     K2KH-EVM        XTCIEVMK2X    3.1            94621          
BMC>    [00:00:03]  BMC>    
BMC>

2. Update UCD module

     I encountered "I2C Operation Timeout" when wanted to update the configuration files.

     Here was my console log.

Beginning BMC command script
[00:09:01]  BMC>ver
[00:09:01]  Executing command "ver"
[00:09:01]  
[00:09:01]  BMC Version    EVM Type    EVM Superset    EVM Subset    EVM Version    EVM S/N        UCD Ver
[00:09:01]  1.0.2.5        0.0.0.1     K2KH-EVM        XTCIEVMK2X    3.1            94621          
[00:09:01]  
BMC>
[00:09:01]  BMC>hwdbg cmd i2c
[00:09:01]  Executing command "hwdbg"
[00:09:01]  Enabling command: i2c
BMC>
[00:09:01]  BMC>shutdown pwr
[00:09:01]  Executing command "shutdown"
BMC>
[00:09:04]  BMC>i2c 1.4E D2 04 01 04 10 40
[00:09:04]  Executing command "i2c"
[00:09:04]  The following errors occurred on I2C operations number 0:
[00:09:04]  I2C Operation Timeout
[00:09:04]  The following errors occurred on I2C operations number 1:
[00:09:04]  I2C Operation Timeout
[00:09:04]  The following errors occurred on I2C operations number 2:
[00:09:04]  I2C Operation Timeout
[00:09:04]  The following errors occurred on I2C operations number 3:
[00:09:04]  I2C Operation Timeout
[00:09:04]  The following errors occurred on I2C operations number 4:
[00:09:04]  I2C Operation Timeout
[00:09:04]  The following errors occurred on I2C operations number 5:
[00:09:04]  I2C Operation Timeout
[00:09:04]  Read results: 
BMC>











May I say this K2HEVM need to request Advantech for repair process? Thanks in advance.

B.R.

OC