Hi,
After I use insmod mount remoteproc,
Using this cde download .bin file but it‘s failed
// Standard header files
#include <stdio.h>
#include <sys/mman.h>
#include <fcntl.h>
#include <errno.h>
#include <unistd.h>
#include <string.h>
#define PRU_NUM 0
#define ADDEND1 0x98765400u
#define ADDEND2 0x12345678u
#define ADDEND3 0x10210210u
#define DDR_BASEADDR 0x80000000
#define OFFSET_DDR 0x00001000
#define OFFSET_SHAREDRAM 2048 //equivalent with 0x00002000
#define PRUSS0_SHARED_DATARAM 4
// Driver header file
#include "prussdrv.h"
#define PRU_NUM 0
static int LOCAL_exampleInit ();
static int mem_fd;
static void *ddrMem, *sharedMem;
static unsigned int *sharedMem_int;
int main (void)
{
volatile unsigned long i,j;
unsigned int ret;
printf("\nINFO: Starting %s example.\r\n","test");
/* Initialize the PRU */
prussdrv_init ();
/* Open PRU Interrupt */
ret = prussdrv_open(PRU_EVTOUT_0);
if (ret)
{
printf("prussdrv_open open failed\n");
return (ret);
}
/* Initialize example */
// printf("\tINFO: Initializing example.\r\n");
// LOCAL_exampleInit();
/* Execute example on PRU */
printf("\tINFO: Executing example on PRU0.\r\n");
prussdrv_exec_program (PRU_NUM, "./test.bin");
printf("\tINFO: Executing example done.\r\n");
for(i = 0; i < 5000;i++)
for(j = 0; j < 1000000; j++);
/* Disable PRU*/
// printf("Disable PRU\r\n");
// prussdrv_pru_disable(PRU_NUM);
// prussdrv_exit ();
return(0);
}
/*****************************************************************************
* Local Function Definitions
*****************************************************************************/
static int LOCAL_exampleInit ()
{
void *DDR_regaddr;
/* open the device */
mem_fd = open("/dev/mem", O_RDWR);
if (mem_fd < 0) {
printf("Failed to open /dev/mem (%s)\n", strerror(errno));
return -1;
}
/* map the memory */
ddrMem = mmap(0, 0x0FFFFFFF, PROT_WRITE | PROT_READ, MAP_SHARED, mem_fd, DDR_BASEADDR);
if (ddrMem == NULL) {
printf("Failed to map the device (%s)\n", strerror(errno));
close(mem_fd);
return -1;
}
//FLush the flag locations of PRU0 and PRU1
DDR_regaddr = ddrMem;
*(unsigned long*) DDR_regaddr = 0x00;
DDR_regaddr = ddrMem + 0x000000004;
*(unsigned long*) DDR_regaddr = 0x00;
return(0);
}
please give me some advice
thanks
li