Other Parts Discussed in Thread: SN65HVD232
Hi All,
I have enabled both DCAN0 and DCAN1 interfaces on BBB. I am using the canutils for testing the CAN interface, I am trying to transmit on CAN0 (./cansend can0 5AA#) and receive on CAN1 (candump can1) but I am unable to get any data on CAN1
The kernel log for CAN is as follows:
We have the following setup:
1. A Beagle bone black
2. Two CAN transceivers - SN65HVD232 (For CAN0 and CAN1)
3. A 120ohm terminating resistor ( CANH and CANL of both CAN0 and CAN1 are connected across the resistor).
We have followed the below steps-
1.Loading modules:
root@am335x-evm:~# modprobe can
[ 195.500159] can: controller area network core (rev 20120528 abi 9)
[ 195.506757] NET: Registered protocol family 29
root@am335x-evm:~# modprobe can-dev
root@am335x-evm:~# modprobe can-raw
[ 244.549436] can: raw protocol (rev 20120528)
2. Setting bus restart type for both CAN0 and CAN1:
root@am335x-evm:~# ip link set can0 type can restart-ms 100
3.Setting bitrate and making both CAN interfaces up:
root@am335x-evm:~# ip link set can0 up type can bitrate 125000
[ 370.223226] c_can_platform 481cc000.d_can can0: setting BTR=1c0b BRPE=0000
4. Sending data on CAN0
root@am335x-evm:~/install/bin# ./cansend can0 5A1#11.2233.44556677.88
root@am335x-evm:~/install/bin# [ 1585.887401] c_can_platform 481cc000.d_can can0: setting BTR=1c0b BRPE=0000
But I am unable to receive data on CAN1.