Other Parts Discussed in Thread: 66AK2H06
Hi
I would like to configure a Keystone II system in such a way that each DSP's have their own ip address. My goal is to be able to send ip packets between linux running on the ARM side and each of the DSP cores. I would also like to use standard sockets when sending/receiving packets on the linux side. What configurations are necessary to achieve this?
My initial thought is that I will need to configure the Packet Accelerator to forward the different DSP addresses to separate queues, but what configurations are necessary to do in the Gigabit Ethernet Switch. Would I need to add ALE entries for each DSP ip address? Does the Gigabit Ethernet Switch support the case where a packet arrives at Port 0 (Host Port) and should be routed back to the same port?