Hello,
I was using Blackhawk USB560m to download binary file to DM6446 and debug it. I set a break point when the DSP was running. Then I closed CCS 3.3 and turned off the DSP board. However, when I turned on the DSP and tried to run downloaded program on the DSP through CCS 3.3 and Blackhawk USB560m emulator, an error occured. The picture above shows the error message. Also, the messages appeared in red on CCS are as follows.
"Trouble Halting Target CPU: Error 0x00000020/-1060 Error during: Execution, An unknown error prevented the emulator from accessing the processor in a timely fashion. It is recommended to RESET EMULATOR. This will disconnect each target from the emulator. The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target. Sequence ID: 15 Error Code: -1060 Error Class: 0x00000020"
"Failed to remove the debug state from the target before disconnecting. There may still be breakpoint opcodes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging."
I turned off the DSP board, the Blackhawk emulator and closed CCS 3.3 and tried again. But it did not help. I also reset the emulator using CCS 3.3. It did not help, neither.
Binary files can be downloaded to DSP. But it seemed that the DSP was totally out of control. It did not respond to any instructions like run and stop.
Does anyone know how to solve this problem?
Thanks in advance.
Rooter