Hi Forum,
So I have been going thru the Sitara and OE labs and have built the minimal filesystem. I am trying to use the create_sdcard.sh script and not having much luck. Im running it from the ti-sdk-am335x-evm-07.00.00.00/bin folder. If I have it use the prebuilt images (option 1 after partitioning) from the sdk it work with no problems. If I have it use a custom boot and rootfs I run in to a bunch of troubles.
When I run it Im giving it the path to the deploy/images folder. Im using that directory for each of the three times it asks for a directory or files. All the file are in there I think. Its the files that are built from the Arago setting up the build environment page. I have also tried moving the needed files out of there into their own directory and not had any luck. See attached output from the script and my directory lists. Anyone have any suggestions what to try or change?
Thanks
Matt