Hi,
I have one question regarding WEC7 build setting.
My customer uses WEC7 with AM3517.
Customer would like to load the OS from NAND flash to DDR2 memory by DMA transfer.
As you know, When building OS, generated file is only one file that is compressed. When booting OS, the compressed file is extracted and loaded. The files are multiple blocks. The head of the block shows the load address. Now the load address are involved odd address.
However, according to some restrictions, destination address of DMA transfer must be even address on customer's system. So customer would like to fix the load address to be even address only. Are there any way to fix the load address is even address? Is there some build options, and so on?
I appreciate your quick reply.
Best regards,
Michi