This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

question about MSMCSRAM's memory allocation

Expert 2985 points


Hi all,

The FPGA transfers data to DSP through SRIO DIO using SWRITE packet. In FPGA, I just set the Address of SWRITE packet to 0x0C000000 to write the data to DSP's MSMCSRAM. 

But I had set some sections to MSMCSRAM in CMD file.

How to avoid these sections not to cover the 0x0C0000000(llength may be 0x1000 bytes)?

Regards,

Feng

  • Hi Feng,

    Try to change the MSMCSRAM base address 0x0c000000 to 0x0c001000 in .cmd file.

    MEMORY
    {
        L1PSRAM (RWX)  : org = 0x0E00000, len = 0x7FFF
        L1DSRAM (RWX)  : org = 0x0F00000, len = 0x7FFF 
    
        L2SRAM (RWX)   : org = 0x0800000, len = 0x080000
        MSMCSRAM (RWX) : org = 0xc010000, len = 0x200000
        DDR3 (RWX)     : org = 0x80000000,len = 0x10000000
    }
    
    SECTIONS
    {
        .csl_vect   >       MSMCSRAM
        .text       >       MSMCSRAM
        GROUP (NEAR_DP)
        {
        .neardata
        .rodata 
        .bss
        } load > MSMCSRAM
        .stack      >       MSMCSRAM
        .cinit      >       MSMCSRAM
        .cio        >       MSMCSRAM
        .const      >       MSMCSRAM
        .data       >       MSMCSRAM
        .switch     >       MSMCSRAM
        .sysmem     >       MSMCSRAM
        .far        >       MSMCSRAM
        .testMem    >       MSMCSRAM
        .fardata    >       MSMCSRAM
        platform_lib > 		MSMCSRAM
    }
    

    For more information refer platform test example in MCSDK package.

    MCSDK Path: "\ti\pdk_C6678_1_1_2_6\packages\ti\platform\evmc6678l\platform_test"

    Thanks,