This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

internal RAM testing (DFT)

Hi,

The internal RAM testing has to been done at startup.

Although I did not find any informtion in the docs.

The AM335x technical reference manual mentions :

"DFT

Integrated PBIST controller to test L2 tag and data ram, L1I and L1D data ram and OCM RAM."

It mentions several times to refer to the DFT specs which I did not succeed to find. DFT seems to be only related to USB part.

* How to do this test ? Can we use DFT/PBIST controller for this ?

* Where can I find more information on it ?

Thanks and Regards,

  • Hi,

    Where do you intend to load the program to do this? The ROM code uses internal RAM to load the first-stage bootloader and run it from there.

  • Hi,

    Regarding :

    "• DFT
    – Integrated PBIST controller to test L2 tag and data ram, L1I and L1D data ram and OCM RAM. "

    As it's stated in the SPRUH73j, there is a integrated PBIST on the OCM RAM. In my project , I need to test the internal RAM of 64K (OCM RAM) for medical certification.  

    But there is no information in the datasheet concerning the PBIST on the OCM RAM.

    I just need some information, to know how work this PBIST, how could I use it to fulfill my test functionality, if it's possible to use it.
    I understand that the first stage of the bootloader is done in this memory.

    Thanks,

  • I suggest you contact your nearest TI representative about this use case.

  • Hi Zanzibar

    This is a documentation escape. PBIST and DFT features are for TI internal testing only. There is no plan to enable use of these feature for customers. 
    I will submit a documentation bug to have these features removed from the documentation to avoid confusion. 

    Regards

    Mukul