Other Parts Discussed in Thread: AM3356, AM3359
Hello,
I'm looking for some insight into the hardware interfacing to Ethernet MAC's on the AM3356 actually. The V1.0 version of the AM3359 ICE board had MIIx connections straight from the AM3359 to the two MAC's. On the V2.1 AM3359 ICE board there's some "muxing" going on between the AM3359 and the MACs. I'm looking for some insight into what's going on here. In my application I need to connect to a 10/100/1000 PHY on one MII port through the PRU unit, and a second MII port to a 10/100 MAC connected to a fibre transceiver. These are separate interfaces, I do not need to 'bridge' these. So is there any reason to include the muxing circuitry of the V2.1 ICE design on my board?
Regards,
-Jeff